Technical FAQs

Ask a Question

What size knockouts are supplied with the 9001SKY enclosures?

9001 SKY1, 2, 3, 4, and 6 have a 0.75 inch diameter conduit entry.
9001 SKY9, and 12 have a 1.0 inch diameter conduit entry. 9001 SKY16, and 20 have a 1.5 inch diameter conduit entry. The 9001 SKY25 has two 1.5 inch diameter conduit entries.

All conduit entries are located in the bottom of the enclosures and have conduit hubs furnished.


CTA-ID : 2004639
Was this helpful?
What can we do to improve the information ?