Technical FAQs

Ask a Question

What does Square D offer in hospital clock and elapsed time meters?

Square D offers a digital dual display clock/timer is catalog number MCT-12B and it`s optional remote control unit, catalog number MCT-CT (with integral battery back-up,) and if the remote control is not required, an optional battery back-up, catalog number MCT-BP, is available to hold the clock and timer settings, though not the display, during a loss of power event.

Square D also offeres a Surgical Chronometer, catalog number MCT-14B, which is a digital clock with three timers. The control panel, catalog number MCT-4RC is required with the MCT-14B. The control panel come with the battery back-up integral to the unit.

These can be found on pages 53, 54, and 55 of the Hospital Isolate Power Systems catalog, document # 4800CT9801


CTA-ID : 2004278
Was this helpful?
What can we do to improve the information ?