Technical FAQs

Ask a Question

Does Square D have a recommendation for a source for the *-gang back boxes required for some of the various Hospital Isolation Panel accessories, such as the 50 series power/ground and ground slave modules, and the MCT-CT clock/timer remote control unit?.

Square D does not recommend any specific gang box manufacturer. It may be necessary to gang together single boxes if the installer is unable to locate the appropriate gang box for the given accessory.


CTA-ID : 2003986
Was this helpful?
What can we do to improve the information ?