Technical FAQs

Ask a Question

What is the torque value for wire binding screw for lug of NSJ?

It is 275 lb.-in. or 31 N-m for both the 32508 and 32510 lugs.


CTA-ID : 2007518
Was this helpful?
What can we do to improve the information ?