Technical FAQs

Ask a Question

How long and what color is the cable provided in kit number XY2CZ9325?

83.7` galavanized steel aircraft control cable with red jacket 1/8`` diameter. This MUST be aircraft control cable, which, as a stranded
cable, will not stretch when pressure is applied. Other types of stranded cable will stretch over time and are not acceptable for this application. Kit also contains four cable clamps, a turnbuckle, cable support, end spring, and three cable end protectors.

CTA-ID : 2035231
Was this helpful?
What can we do to improve the information ?