Technical FAQs

Ask a Question

What float and seal kit comes with 9037HG devices as standard?

304 stainlesss float is 9049HF3 and Buna N seal is 9998PC337 per 9037-891 Instruction Bulletin.

Seals used with forms Z19, 20 and 21 are Viton, 9998PC338.

The 316 stainless steel float used with form Z21 is the 9049HF4


CTA-ID : 2007747
Was this helpful?
What can we do to improve the information ?