Technical FAQs

Ask a Question

What is the Neutral Assembly for a DU324 safety switch?

Issue:
Selection

Product Line:
GD Safety Switch

Cause:
Selection of neutral assembly

Resolution:
The neutral assembly used for the DU324 is dependent upon the Series number of the switch. For Series F1, use SN20A. For Series E2 or E3, use SN225KA. For Series E1, or prior designs, a field installable neutral assembly was not available.


CTA-ID : 2007512
Was this helpful?
What can we do to improve the information ?