Technical FAQs

Ask a Question

Are the LE1UD IEC enclosed starters available with a DC coil?

No but there is room enough in the enclosure for the customer to add an interposing relay with a DC coil. The relay then could pull in the starter.


CTA-ID : 1697
Was this helpful?
What can we do to improve the information ?