Technical FAQs

Ask a Question

Can a QC816F200C, Series M01 Combination Service Entrance Device be upgraded to a higher ampacity main?

No, this CSED devices` wiring diagram states `` MAINS 200 AMP MAX. - SEE SERVICE DISCONNECT FOR RATING``. The 200 ampere QOM2200VH main breaker installed is the maximum ampacity allowed

CTA-ID : 2006809
Was this helpful?
What can we do to improve the information ?