Technical FAQs

Ask a Question

Can a QC816F150C, Series M01 Combination Service Entrance Device be upgraded to a higher ampacity main?

Yes, this CSED devices` wiring diagram states `` MAINS 200 AMP MAX. - SEE SERVICE DISCONNECT FOR RATING``. The QOM2-VH main breaker installed can be replaced with a maximum 200 ampere QOM2-VH main breaker.


CTA-ID : 2006807
Was this helpful?
What can we do to improve the information ?