Technical FAQs

Ask a Question

Are test reports available for the NT and NW breakers?

Yes, standard on ANSI, optional on the UL and IEC versions. Suffix will be T.


CTA-ID : 2006669
Was this helpful?
What can we do to improve the information ?