Technical FAQs

Ask a Question

What is the NEMA rating of the D10 switch handles ?

The Handle ratings are NEMA 1, 3, 3R, 4, and 12.


CTA-ID : 2006403
Was this helpful?
What can we do to improve the information ?