Technical FAQs

Ask a Question

What is the maximum size of conductor that can run through a riser load center QO11224L125GWGC or QO12024L125GWGC?

Refer to the NEC code to determine the size of the riser conductor, which is dependent on the total load required, and on the amount of fill allowed for the gutter space of 4`` wide and 3.75`` deep.

CTA-ID : 2006399
Was this helpful?
What can we do to improve the information ?