Technical FAQs

Ask a Question

Is this a valid catalog number? KAL362258077 suffix 8077

The 8077 suffix is obsolete. The PDC6KA4 lug is now only field installed, instead of a factory installed option using suffix 8077.


CTA-ID : 2006797
Was this helpful?
What can we do to improve the information ?