Technical FAQs

Ask a Question

Can a RC816F200CH, Series M01 Combination Service Entrance Device be upgraded to a higher ampacity main?

Issue:
Product design features

Product Line:
Combination Service Entrance Devices

Environment:
Mains rating

Cause:
Application

Resolution:
No, this CSED devices' wiring diagram states "MAINS 200 AMP MAX. - SEE SERVICE DISCONNECT FOR RATING". The 200 ampere QOM2200VH main breaker installed is the maximum ampacity allowed


CTA-ID : 2006778
Was this helpful?
What can we do to improve the information ?