Technical FAQs

Ask a Question

What is the part number for the 2510 KO6C stainless steel flush plate ?

Order the 9999 PL13 pilot light and the 2510 KO6 switch separately. The standard flush plate without the lens is part number 31058-007-04. The jumbo plate is 31058-006-05.


CTA-ID : 2006397
Was this helpful?
What can we do to improve the information ?