Technical FAQs

Ask a Question

Can the Powerbus 225 busway be mounted flatwise so that the plugs are pointing either up or down?

The bus can be mounted flatwise. The busway support requirements change to 5 ft maximum centers and the plug in units do not retain the IP54 enclosure rating. There is no standard hanger available to mount the busway in the flatwise position.

CTA-ID : 2006395
Was this helpful?
What can we do to improve the information ?