Technical FAQs

Ask a Question

What is the wire range of the main lugs supplied in the QOM22225NF circuit breaker enclosure?

The actual wire range of the lugs used is #6 AWG - 300 kcmil, aluminum or copper conductors. However, the wire bending space provided in the enclosure restricts the conductors to 250 kcmil.

CTA-ID : 2006771
Was this helpful?
What can we do to improve the information ?