Technical FAQs

Ask a Question

Can you turn instantaneous off with the Powerpact R breakers? Is there an instantaneous override?

As long as the trip unit has short-time, instantaneous can be turned off. Instantaneous override values are in Class 612 catalog.


CTA-ID : 2006759
Was this helpful?
What can we do to improve the information ?