Technical FAQs

Ask a Question

What are the repair parts for a QO330MQ150, Series S3, Load Center?

Only the parts listed below are considered field replaceable.
Cover - QOC342MQF or QOC342MQS
Interior Assembly - QO330M150I
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QDL32150
Main Circuit Breaker Connecting Strap - 4055901903 (3 req`d)
Main Circuit Breaker Connecting Strap Mounting Keps Nut - 2342702001 (3 req`d)
Indoor Cover Mounting Screw - 4020513002K (6 req`d)
Indoor Cover Door Hinge - 4028356450K (3 req`d)
Door Latch Kit - 4020284450K


CTA-ID : 2006556
Was this helpful?
What can we do to improve the information ?