Technical FAQs

Ask a Question

What is the NEMA rating for the enclosed non-metallic Vario loadbreak switch?

These enclosures are rated IP55, NEMA 1 and NEMA 12.

Please note: This does not apply to the enclosed Mini-Vario switches
(VCFN12GE & VCFN20GE) which are rated IP55 only and are not UL Listed.

CTA-ID : 2006383
Was this helpful?
What can we do to improve the information ?