Technical FAQs

Ask a Question

What is the Terminal Lug Data for a DJM circuit breaker used in an EZMK332400 branch device?

The standard lug, catalog number 32508, accepts (1) #2 AWG - 600 kcmil copper or (1) #2 AWG - 500 kcmil aluminum conductor.

CTA-ID : 2006755
Was this helpful?
What can we do to improve the information ?