Technical FAQs

Ask a Question

Can a QO2150, QO2175, QO2200 or QO2225SL be used in CSED All-In-One devices?

These breakers can be used in the following CSED All-In-One devices:
QC2442M150CH, QC2442M200C and QC2442M200CH.
NOTE: The branch circuit breaker ampacity cannot exceed the CSED mains ampacity rating.

CTA-ID : 2006537
Was this helpful?
What can we do to improve the information ?