Technical FAQs

Ask a Question

Does Square D offer any of the QO, single phase load centers (for example a QO140M200) with the cover included?

Issue:
Product Design Features

Product Line:
QO load centers

Cause:
Application

Resolution:

Yes, SEE THE CURRENT ON-LINE DIGEST PLUS FOR CATALOG NUMBERS. For example a QO140M200C will have a combination cover (use for flush or surface mount applications) included with the load center.


CTA-ID : 2006309
Was this helpful?
What can we do to improve the information ?