Technical FAQs

Ask a Question

Is the 9065 SFC20 interchangeable with the 9065 SFO20 ?

Yes. In fact, the 00, 0 & size 1 are all interchangeable because they`re the same physical size.


CTA-ID : 2006740
Was this helpful?
What can we do to improve the information ?