Technical FAQs

Ask a Question

QO2200: Can this be applied in an NQOD panelboard?

No, this breaker is not UL listed or warranted for application in an NQOD panelboard.

The launch document states that these devices are for use in single phase load centers and CSED only!!!



CTA-ID : 2006527
Was this helpful?
What can we do to improve the information ?