Technical FAQs

Ask a Question

What is the replacement pull ring and latch spring for QOC440MF or QOC440MS?

Issue:
Old Obsolete repair parts

Product Line:
QO Load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: The covers are both obsolete, NLA, with no replacements.

But the Pull ring is part #4055307301 and the Latch Spring is part number 4055307201. SEE BELOW FOR A VISUAL OF EACH


Was this helpful?
What can we do to improve the information ?