Technical FAQs

Ask a Question

When adding an X suffix to an EZMR branch device catalog number, designating an increase from 800 ampere to 1200 ampere cross bus rating, does the device dimensions change?

No, the enclosure dimensions do not change when an X suffix is added to the EZMR branch device catalog number.

CTA-ID : 2006520
Was this helpful?
What can we do to improve the information ?