Technical FAQs

Ask a Question

When adding an X suffix to an EZMH branch device catalog number, designating an increase from 800 ampere to 1200 ampere cross bus rating, do the dimensions of the device change?

No, the enclosure dimensions do not change when an X suffix is added to the EZMH branch device catalog number.

Was this helpful?
What can we do to improve the information ?