Technical FAQs

Ask a Question

Can a QO breaker trip when handle is locked in the ``ON`` position?

Yes. All QO breaker are ``trip-free`` even when toggle/handle is locked in the on position. This is a UL requrirement.


CTA-ID : 2006347
Was this helpful?
What can we do to improve the information ?