Technical FAQs

Ask a Question

Are we obsoleting all FD, FG, FJ circuit breakers?

All FD, FG, FJ circuit breakers have been placed into obsolescence with the exception of FJ 480Y/277 Vac 1-pole 15-70 amp circuit breakers. The FJ 1-pole circuit breakers will be offered because there is not a 1-pole FC circuit breaker.


CTA-ID : 2006337
Was this helpful?
What can we do to improve the information ?