Technical FAQs

Ask a Question

Is an additional neutral lug or equipment ground lug, available for use when a HOM2150BB, HOM2175BB or HOM2200BB branch circuit breaker, or HOML2225 sub feed lug kit is used in a Homeline load center?

Product accessories

Product Line:
Homeline load centers



A neutral lug kit, LK225AN, is provided with these branch circuit breakers, for field installation on the load centers neutral bar. In most applications, a standard equipment ground bar will be able to terminate the circuits equipment ground conductor. If an additional equipment ground lug may be required, order LK100AN separately, for field installation on a standard equipment ground bar.

CTA-ID : 2006517
Was this helpful?
What can we do to improve the information ?