Technical FAQs

Ask a Question

What lugs are available for use in a 300 ampere or 400 ampere Combination Service Entrance Device?

Lug options listed on the device wiring diagram include: Mechanical lugs - Square D CMELK4 (includes four ILSCO TA-600-2N lugs in kit), ILSCO TA-600-2N or Anderson L2D2-350: Compression lugs - Anderson VHCL-600-12BN.


CTA-ID : 2006722
Was this helpful?
What can we do to improve the information ?