Technical FAQs

Ask a Question

What is the maximum amperage of branch circuit breaker that can be installed in a SC816D150C Combination Service Entrance Device?

A 100 ampere maximum branch circuit breaker may be installed in the lowest position in the branch panel. All other branch positions are limited to a 70 ampere maximum branch circuit breaker.


CTA-ID : 2006640
Was this helpful?
What can we do to improve the information ?