Technical FAQs

Ask a Question

What is the maximum ampere rating of branch circuit breaker that can be installed in a SC816D200C Combination Service Entrance Device?

Issue:
What is the highest ampacity branch breaker that will install in an SC816D200C CSED?

Product Line:
Residential electrical distribution equipment

Environment:  
Square D Combination Service Entrance Devices (CSEDs)

Cause:
Application

Resolution:
A 100 ampere maximum branch circuit breaker may be installed in the lowest spaces in the branch panel. All other branch positions are limited to a 70 ampere maximum branch circuit breaker.
Was this helpful?
What can we do to improve the information ?