Technical FAQs

Ask a Question

Can the high amp branch breakers, HOM2150BB, HOM2175BB or HOM2200BB be used as a back-fed main in a Homeline load center?

Product Design features

Product Line:
Homeline load centers and branch breakers

Back feeding branch breaker


Yes, in Homeline load centers rated 150 ampere or greater. However, the branch breaker ampacity cannot exceed the load center mains ampacity rating. The installation of the breaker as a back-fed main will also require the use of a HOM5RK retaining kit.

CTA-ID : 2006514
Was this helpful?
What can we do to improve the information ?