Technical FAQs

Ask a Question

Are there any limitations in which branch circuit breakers can be mounted next to the HOM2150BB, HOM2175BB, HOM2200BB branch circuit breakers or HOML2225 sub-feed lug kit?

Product limitations

Product Line:
Homeline Branch Circuit Breakers and Sub-Feed Lug kits

Branch breaker mounting



Yes, due to the size of the load conductors and their exit parallel to the side wall of the load center enclosure, certain branch circuit breaker ampacities cannot be mounted next these branch breakers. Please refer to the Installation Bulletin supplied with the branch circuit breaker or sub-feed lug kit for clarification of the restrictions.

CTA-ID : 2006511
Was this helpful?
What can we do to improve the information ?