Technical FAQs

Ask a Question

Is the MM125MB or MM200MB Slider Type Manual Circuit Closer suitable for continuous duty?

No, these devices are for temporary use only. For a meter socket closing plate with continuous duty jumpers, contact Ekstrom Industries, Inc at 800-523-4332 or 248-477-0250.


CTA-ID : 2006310
Was this helpful?
What can we do to improve the information ?