Technical FAQs

Ask a Question

Can the QO318L200G, Fixed Main Lugs Only, load center be converted to a Main Breaker load center?

Issue:
product features

Product Line;
QO load centers

Environment;
Convert to main breaker

Cause:
Application

Resolution;
This is a fixed Main Lug load center and is not convertible to a Main Breaker load center.
 
Was this helpful?
What can we do to improve the information ?