Technical FAQs

Ask a Question

Can a D326NT be modified to accept Class R fuses?

No, this device accepts 300Vac Class T fuses only. If Class R fuses are required, an option is using a D326N safety switch and a DRK600 Class R Fuse Kit.


CTA-ID : 2006621
Was this helpful?
What can we do to improve the information ?