Technical FAQs

Ask a Question

Can a D326NTR be modified to accept Class R fuses?

No, this device accepts 300Vac Class T fuses only. If Class R fuses are required, an option is using a D326NR safety switch and a DRK600 Class R Fuse Kit.

CTA-ID : 2006622
Was this helpful?
What can we do to improve the information ?