Technical FAQs

Ask a Question

Does Square D offer a Computer Network Router in the Multi-Link product line?

Yes, we offer a SDM7DR, a 7 port router/ethernet hub. This device allows multiple computers located within the LAN (Local Area Network) to share cable or DSL internet service. It also serves as a 10/100 BASE-T ethernet hub to create the LAN. It provides a security firewall to protect your computers from outside hackers (masks your IP address from others on the internet). Supports both PC and Mac operating systems.

CTA-ID : 2006497
Was this helpful?
What can we do to improve the information ?