Technical FAQs

Ask a Question

Do circuit breakers for Service Entrance have to be 100% rated?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
Circuit breakers in service entrance applications do not need to be 100% rated. 

NOTE: 

Circuit breakers are not service entrance rated.  Service entrance rating goes with the enclosure or panel.
 
Was this helpful?
What can we do to improve the information ?