Technical FAQs

Ask a Question

Can a D325NT be modified to accept Class R fuses?

No, this device accepts 300Vac Class T fuses only. If Class R fuses are required, an option is using a D325N safety switch and a DRK40 Class R Fuse Kit.


CTA-ID : 2006618
Was this helpful?
What can we do to improve the information ?