Technical FAQs

Ask a Question

The QOM2 frame main circuit breaker used in the Homeline load centers seem to be difficult to operate to the ON position. Is this normal?

Issue:
Product characteristics

Product Line:
Load Center Main Breaker

Cause:
Difficulty turning the breaker ON

Resolution:
The extra force required to turn the circuit breaker ON, as compared to the force required to turn the circuit breaker OFF, is normal. The operating handle of the QOM2 main circuit breaker requires 24 lbs of force to turn ON, 7 lbs of force to turn OFF and 10 lbs of force to RESET.


CTA-ID : 2006483
Was this helpful?
What can we do to improve the information ?