Technical FAQs

Ask a Question

What is the difference between AL100TF lugs and other lugs typically applied in F frame circuit breakers?

1. AL100TF lugs are applied only on the off end of the breaker when the off end is the load end.
2. The wire binding screw is accessed from the end of the breaker, that is, the place where normally the conductors are brought into the breaker.
3. The conductors are brought into the lugs where normally the wire binding screw is accessed, that is from the front surface of the breaker.


CTA-ID : 2006474
Was this helpful?
What can we do to improve the information ?