Technical FAQs

Ask a Question

With regard to the new style (Series S03) QO 3-phase main breaker load centers and covers, why did the catalog numbers, versus only the series numbers, of the load centers and covers change?

Since the covers are merchandised separately, the catalog numbers had to be changed to allow customers to match the correct load center with the correct cover.


CTA-ID : 2006273
Was this helpful?
What can we do to improve the information ?