Technical FAQs

Ask a Question

What are the repair parts for the H361WA, series F6 (may be shown as F06)?

The repair parts for the H361WA, series F6 (F06) are as follows. No other parts are available.
-Line Base Assembly -4056603950 (requires one per switch. Arc suppressor assembly not included)
-Load Base Assembly - 4056604150 (requires one per switch)
-Line and Load Base Mounting Screw - 4020515101(3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Handle Assembly - 4056663550
-Switch Mechanism - 4056787350
-Rod/Linkage Assembly - 4056787050
-Lug Kit - AL0306F (one kit includes all line and load lugs)
-Receptacle - WRDK3034 (mounting screws included)


CTA-ID : 2006597
Was this helpful?
What can we do to improve the information ?