Technical FAQs

Ask a Question

What are the repair parts for the HU361AWC, series F7 (may be shown as F07)?

The repair parts for the HU361AWC, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056609150 (requires one per switch. Arc suppressor assembly not included)
-Line Base Mounting Screw - 4020515101(3 required)
-Arc Suppressor Assembly - 4056635550 (requires one per switch)
-Arc Suppressor Mounting Screw - 4020514501
-Lug Assembly - 40251-016-52 (per lug)
-Lockplate - 4056672101 (NOTE: Handle Assembly Gasket may also need replacing)
-Lockplate mounting screw - 2299940562 (2 required)
-Handle Assembly - 4056663550 (also recommend replacing Handle Assembly Gasket)
-Handle Assembly Gasket - 4056603101
-Switch Mechanism - 4056787350 (also requires Switch Mechanism Gasket and Switch Mechanism Washer. NOTE: Handle Assembly Gasket may also need replacing)
-Switch Mechanism Gasket - 4056786001
-Switch Mechanism Washer - 2360200008
-Rod/Linkage Assembly - 4056787050
-Receptacle - 2541002806
-Receptacle Mounting Screws - 4510280101 (required 4)


CTA-ID : 2006596
Was this helpful?
What can we do to improve the information ?