Technical FAQs

Ask a Question

The HOM816L125C load center uses a HOMC12UC cover. Why doesn`t the cover catalog number reflect the number of circuits in the panel?

Issue:
Product Features

Product Line:
Homeline Load Center

Cause:
Clarifiying product design features

Resolution:
The cover is a common cover, used on more load centers than the HOM816L125C. The HOMC12UC catalog number does indicate that there would be openings in the covers dead-front trim for 12 branch circuit breakers. When used with the HOM816L125C load center, a maximum of eight of the circuit breaker openings would be utilized.


CTA-ID : 2006594
Was this helpful?
What can we do to improve the information ?